在LMX2592的datasheet中reference input signal 在ac耦合情况下,单端输入时,幅度最小值为0.2Vppd,幅度最大值为2Vppd。
这里有两种理解:1.输入信号的最大值只要大于0.2Vppd,小于2Vppd,最小值大于0V
2. 0.2v<输入信号幅度<2v 最大值小于2Vppd,最小值大于0.2v
在8.1.3节又有说标准的时钟输入:LVDS/LVPECL/HCSL/CMOS都可以
该如何理解LMX2592对输入参考信号幅度的要求?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在LMX2592的datasheet中reference input signal 在ac耦合情况下,单端输入时,幅度最小值为0.2Vppd,幅度最大值为2Vppd。
这里有两种理解:1.输入信号的最大值只要大于0.2Vppd,小于2Vppd,最小值大于0V
2. 0.2v<输入信号幅度<2v 最大值小于2Vppd,最小值大于0.2v
在8.1.3节又有说标准的时钟输入:LVDS/LVPECL/HCSL/CMOS都可以
该如何理解LMX2592对输入参考信号幅度的要求?
在8.1.3节又有说标准的时钟输入:LVDS/LVPECL/HCSL/CMOS都可以.
这里的LVDS/LVPECL/HCSL/CMOS指的是时钟信号的输入可以接受的电平标准,即 OSCinM 和OSCinP信号。
而 0.2Vppd<Vin<2Vppd指的是输入信号的幅值范围。
是的,单端输入的话,保证0.2Vppd<Vin<2Vppd
如果差分输入的话,那么每个单端信号的范围就是0.1Vppd<Vin<1Vppd. 因此Vid即为0.2Vppd<Vin<2Vppd