在使用TXS0108E这款8位双向电压电平转换芯片时,受到一些限制只能A-3.3V转B-3.3和5V,并不能转1.8V。有其他芯片方案能实现三个转换吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用TXS0108E这款8位双向电压电平转换芯片时,受到一些限制只能A-3.3V转B-3.3和5V,并不能转1.8V。有其他芯片方案能实现三个转换吗?
可以参考SN74LVC8T245,可以实现1.8V,3.3V以及5V之间的电平转换。
还发现一个问题,为什么TXS0108E A端输入1.8V信号 B端并不能转出3.3V的信号,但是B端输入3.3V的信号,A端却能输出1.8V的芯片?芯片不是应该是双向的吗?怎么会是单向的?但是我换TXS0104E 四路的确两边都可以?会不会是我买到假芯片了?
SN74LVC8T245好像需要控制DIR方向的,有无需控制的方向的,能支持3.3V同时转1.8V\3.3V\5V 八路的芯片吗?