这是芯片手册给出的单个IO输出电流相关参数
芯片VCCA侧采用3.3V供电,VCCB侧采用5V供电,如果VCCB方向从A到B,B侧每个IO输出,且同时输出,最大电流32mA。这样8个IO总共需要250mA电流
但是下面给出的IO最大才100mA,这样会不会有问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这是芯片手册给出的单个IO输出电流相关参数
芯片VCCA侧采用3.3V供电,VCCB侧采用5V供电,如果VCCB方向从A到B,B侧每个IO输出,且同时输出,最大电流32mA。这样8个IO总共需要250mA电流
但是下面给出的IO最大才100mA,这样会不会有问题?