Hi,
目前我有一配置問題想請教:
目前我948的SEL0为1.25V,SEL1为0.8V,947对应的SEL0和SEL1设定的电压应该是多少?
不清楚947'要怎麼配置。
另外,这种传输需要更改软件的么?本来我的软件直接驱动液晶屏是可以的,现在中间见了这个947-948,软件上需要调整么?
謝謝
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
目前我有一配置問題想請教:
目前我948的SEL0为1.25V,SEL1为0.8V,947对应的SEL0和SEL1设定的电压应该是多少?
不清楚947'要怎麼配置。
另外,这种传输需要更改软件的么?本来我的软件直接驱动液晶屏是可以的,现在中间见了这个947-948,软件上需要调整么?
謝謝
948配置的SEL0 为1.241V这栏里说明output mode为Dual OLDI output,因此947 对应的OLDI_DUAL=1 才对。然后您再根据自己的实际需求选择AUTO_SS和AUTO_SS 是否enable or disable,1 的话即为enble, 0 即为disable。
同样,948 的SEL1选择的是0.8V,即cable选择是STP ,对应947中的话,那就是coax=0 ,然后再通过MAPSEL 来选择data mapping的情况是0 还是1, 从而确定了SEL1的配置。