This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822IFRHBR LED_0 bootstrap设置冲突的问题/电口光口的问题

大家好,

我在应用中对DP83822IFRHBR有三个问题:

1、LED_0引脚bootstrap的设置

         应用中PHY设置为半双工/全双工自适应,此时AN_0=1,即LED_0的bootstrap必须选择MODE4。由于LED_0内部有50K的默认上拉,MODE4时,该引脚外部上下拉均是OPEN(既无上拉也无下拉)。

         当LED_0用作指示灯控制时,上电时默认带并行上拉电阻,则输出低电平有效;默认带并行下拉电阻则输出高电平有效。并行上下拉电阻的取值范围为1.96K~2.49K。

         从上文两点来看,半全双工设置和LED极性设置可能会产生冲突。

         情形一:LED_0外部不带上下拉电阻,此时选中MODE4,即半/全双工自适应;由于内部自带50K上拉电阻,LED极性设置为低电平输出有效。

         情形二:LED_0外部带2.49K并行上拉电阻,此时选中MODE4,即半/全双工自适应;由于引脚内部和外部均为上拉电阻,LED极性设置为低电平输出有效。

         情形三:LED_0外部带2.49K并行下拉电阻,此时选中了MODE1,只支持半双工;由于平行下拉电阻较小,LED极性设置为高电平输出有效。

         上述3种情形分析的对不对?在半双工/全双工自适应的应用中,是否选择情形一或情形二均可,或者说推荐使用情形二?

 

2、电口和光口芯片的选择

DP83822IFRHBR是否即可支持电口,也可支持光口?还是说DP83822IFRHBR只支持光口?

 

3、MII接口的选择

在bootstrap中,RMII_EN=0,同时RGMII_EN=0时,就是选中MII接口?

有熟悉这款PHY芯片的朋友帮忙解答一下,谢谢!