你好,目前我们想使用DS90UB953A-q1与索尼的IMX385进行对接,发现IMX385传感器与IMX390不一样,IMX385工作时需要RESET、HS、VS、CLK、IIC等信号,这些信号怎么由解串器端发送过来了? 或是DS90UB953A-q1与索尼的IMX385不能直接对接,需要在前端增加外围控制芯片?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,目前我们想使用DS90UB953A-q1与索尼的IMX385进行对接,发现IMX385传感器与IMX390不一样,IMX385工作时需要RESET、HS、VS、CLK、IIC等信号,这些信号怎么由解串器端发送过来了? 或是DS90UB953A-q1与索尼的IMX385不能直接对接,需要在前端增加外围控制芯片?
您好,DS90UB953A 输入的是MIPI信号,IMX385 有HS, VS,输出的是RGB信号吗?要看下sensor输出什么信号,然后再看使用什么serializer型号。
你好,我看了sensor输出的MIPI数据格式为RAW10或是RAW12,不知道DS90UB953A(只能对接RGB数据吗?)是否可以对接,GPIO是否可以接HS,VS这些信号呢?谢谢
您好, DS90UB953 的输入是支持4lane mipi 输入信号的, 所以953 和IMX385 对接是可以的.
另外, IMX385 需要的HSYNC, VSYNC, 是可以通过processor ISP的输出经过954 的GPIO 传输到953 的,这个过程是可以的.
954 的datasheet中有相关描述:Each FPD-Link III interface includes a separate low latency bidirectional control channel (BCC) that
continuously conveys I2C, GPIO, and other control information. GPIO signals purposed for sensor synchronization and diagnostic features also make use of the BCC.
另外,就是需要注意的是,参考954 的 datasheet Page40 关于back channel GPIO的时序, GPIO最大能够支持的频率为416KHz, jitter最大为0.7us, 所以需要看下是否满足您的需求,如果可以的话,那么sync就可以通过back channel的GPIO进行传输.
你好,感谢你的回复。
如你所说IMX385 需要的HSYNC, VSYNC, 可以通过processor ISP的输出经过954 的GPIO 传输到953 的,这个过程是可以的。
那么我再由953的GPIO输出给imx385,这样应该也是可行的是吗?谢谢