This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP410使用问题,DVI输出挑显示器

Other Parts Discussed in Thread: TFP410

配置原理如图,不使用I2C,显示器I2C经过电平转换直接接到CPU。ISEL为低,PD及EDGE上拉至3.3V。

现象如下:使用惠普的一款显示器能够正常显示。

使用飞利浦/AOC的显示器,无DVI输出,测量信号,DVO信号正常,DVI输出信号幅值很小,且幅值周期性的上下摆动。(包括DDC 的CLK、SDA信号同样在3.5V~3.7V规律性的上下摆动)使用上述显示器,VGA接口接上一个输入信号源,DVI显示则正常。

请问是哪里有问题?

  • 您好,首先两种不同的显示器,输入源都是同样的吧?那么输出应该也是一样的,断开显示器,直接在TFP410端测量输出信号,看波形是否正常?两种DVI接口的显示器是否有spec,看下差异在哪里? 因为相同的VGA输入源,对于TFP410来说输出应该是一样的。
  • 输入源一样。断开显示器,TFP410无输出了。
  • 断开显示器,测量TFP410 的输出也是应该有信号输出的。跟您确认几个问题:
    1.ISEL/RESET# 需要为low,disable I2C。
    2. 输入如果是24bitRGB形式,BSEN/SCL需要为高。
    3. 参考Table 1,确认DSEL/SDA 如何接的。
    4. DE信号时序正确吗? 或者说不使用I2C的话, 是不是前端视频源有提供DE信号?
  • 1.ISEL/RESET# 下拉到GND。

    2. 输入是24bitRGB形式,BSEN/SCL为高。

    3. DSEL/SDA 下拉到GND。

    4. 前端视频源有提供DE信号。附件是整个TFP410的设计原理图

    2K1000_T10COMe _ P08.pdf

  • 经过接显示器,对所有信号对比测试,发现11脚,MSEN接有显示的显示器时为高,没显示的显示器时为低(拔掉DVI插头也为低),其他信号都一样,就是DVI没有输出信号。

  • 您好,看下MSEN的输出引脚定义:  When I 2C is disabled (ISEL = low), a low level indicates a powered on receiver is detected at the differential outputs. A high level indicates a powered on receiver is not detected. This function is only valid in dc-coupled systems.

    意思是说当MSEN输出为低时,说明已经上电的DVI receiver 被检测到已经连接到DVI transmitter TFP410的DVI差分输出端了,为高电平时,则说明没有检测到monitor连接到DVI的差分输出端,这个功能有效只是在DC耦合系统中适用。 所以看似和您测试的结果相反。

    看了下TFP410 部分的原理图,strapping pin的引脚配置没有问题。

    IDCK频率是多少? 飞利浦的显示器分辨率是多少?

    手头上只有一块TF410的板子吗? 换个板子再和飞利浦的显示器接呢?

  • 从MSEN定义来看,和现象相反。

    另外:The receiver sense input (RSEN) bit indicates if a DVI receiver is connected to TXC+ and TXC-. The HTPLG bit reflects the current state

    of the HTPLG pin connected to the monitor via the DVI connector. When I2C is disabled (ISEL=0), the RSEN value is available on the MSEN pin

    RSEN: This read only register contains the receiver sense input logic state, which is valid only for dc-coupled systems.
    0: A powered-on receiver is not detected
    1: A powered-on receiver is detected (i.e. connected to the DVI transmitter outputs)

    好像这段解释又和现象吻合。就是现在来看,没有显示的时候,msen脚为低电平。

    IDCK频率为100MHz,换过同样规格的板子,现象一样。换过AOC,现象同飞利浦。惠普的显示器显示正常。

     

  • 飞利浦的显示器换了根短点的线缆,有显示了,是不是跟信号匹配有点关系,我翻看之前的帖子,有这么一段,我是TPF410的DVI输出直接接外部显示器的,是不是也需要加匹配电阻。

  • 不接匹配电阻,输出也是应该有信号的,只是眼图波形不好。
    但是DVI,HDMI的输出确实需要在靠近connector端加上匹配电阻。
    您看下飞利浦的显示器和之前能显示的显示器Spec,对比下,是不是能显示的显示器内部已经集成100ohm匹配电阻,而飞利浦的没有呢?
    如果没有的话,建议加上。