您好!
RS232接口芯片MAX3232有4个外部电容,从相关的DLP参考原理图中发现,其使用了耐压为50V的电容,
希望说明一下,为什么需要50V耐压的电容?
芯片datasheet中,对这4个电容(C1-C4),有推荐容值,但并未明确写明耐压要求。
芯片最大规格中,V+和V-的值分别为+7V和-7V,由此来看,相应的C3,C4,耐压在10V以上就可以满足需要。
而C1+-和C2+-引脚电压,找不到明确规格。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
RS232接口芯片MAX3232有4个外部电容,从相关的DLP参考原理图中发现,其使用了耐压为50V的电容,
希望说明一下,为什么需要50V耐压的电容?
芯片datasheet中,对这4个电容(C1-C4),有推荐容值,但并未明确写明耐压要求。
芯片最大规格中,V+和V-的值分别为+7V和-7V,由此来看,相应的C3,C4,耐压在10V以上就可以满足需要。
而C1+-和C2+-引脚电压,找不到明确规格。
您好,在使用MAX3232的时候,我们需要参考recommended Operating Conditions,所以Vcc的最大电压为5.5V,常用的Vcc电压为3.3V和5V,而+-7V的供电电压是 Absolute Maximum Ratings, 指的最大绝对值电压,这里不是指的功能性测试指标。
关于charge pump的最大耐压值,您的理解是对的,一般至少10V以上,或者16V。这里有有一篇关于232的 charge pump电路的blog,介绍的非常详细,详细对您的问题有很大帮助: