如下使用,会存在烧ISO7821的问题,会测出VISO和VDD短路情况,或者测试出实际VDD低于VISO 0.3V,麻烦帮忙看一下,多谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,看了下您的电路,VISO指的是VCCI,也就是3v3_ISO_DC2和3v3_ISO_IF这两个电压是吗?
这两个电压和3.3V VCCO短路? 因为这款隔离器件隔离的是信号,电压并未隔离,所以电压相等是正常的。
如果有0.3V压差,要测试下前端输出的3v3_ISO_DC2和3v3_ISO_IF电压是多少V。