This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK2711 与10G SFP+光模块互连问题

你好,我当前正在使用TLK2711A,速率为1.6Gbps(16bit,100Mhz),当使用10G SFP+ DAC铜缆(10Gtek,10GSFP+ Passive Copper CableAssembly)时,两端的2711收发正常,但是使用1.25G或者10G SFP+光模块(单模,1310nm)时异常,请问是什么原因,谢谢。

  • 您好,根据您的描述,使用10G SFP+ DAC铜缆收发正常,但是使用10G SFP+光模块(单模,1310nm)异常,和您确认下,光模块是同一个光模块,但是线缆材质不同,导致的通信异常是吗?

  • 光模块不同,10G SFP+ DAC铜缆使用的光模块是10Gtek 的 CAB-10GSFP-P1M:

    Features
     SFF-8431 Compliant
     Broadband serial data rate operation:10 Mbps to 12 Gbps
     Power Level I: 15 mW per cable end
     100 Ohm differential impedance
     Retractable pin latch
     EEPROM signature
     Pull to Release latch design
     360°cable braid crimp
     Enhanced EMI skirt design
     Color options for strain relief and pull tab
     Linear design for use with EDCs
     AC-coupled inputs and outputs
     30AWG to 24AWG cable available

    Applications
     10 Gigabit Ethernet and Gigabit
     Ethernet (IEEE 802.3ae)
     Fiber Channel: 1, 2, 4, 8, and 10GFC
     Infiniband SDR, DDR, and QDR
     Fiber Channel over Ethernet (FCoE)
     Serial data transmission

    而光模块是常用的普通1310nm、1550nm单模,使用光纤互连。10G SFP+光模块也测试了多个厂家,结果都不通。

  • 您好,10G SFP+光模块的输入兼容的是什么电平? 因为TLK2711的输出是VML电平,兼容给PECL电平,我怀疑是否二者的电平不兼容导致,电路是AC耦合吗?可以附上电路看下。
  • 对,我看了之前论坛里也有TLK2711和SFP电平兼容的帖子,我让做硬件的同事回复您,谢谢。
  • 可以的,建议是先查看光模块的datasheet,看下输入兼容的什么电平标准,共模电压是多大。
  • TLK2711输出的电平如下图。而10GHz SFP+ 光模块的共模电压为1.3V,输出电平为CML模式,确实是与2711的电平标准不一致,可差异并不太大。有什么方法可以解决这个问题呢?是要换一个输出是VML电平的光模块还是说有其他方法?另附一张SFP的部分电路图。

  • 您好,我最近也在TLK2711上遇到有些问题,您能加一下我微信吗?1009278482
  • 您好,光模块是输入兼容的VML 电平吧?因为我们要把TLK2711的输出和光模块的输入连接。
    通常情况下,如果输出和输入的共模电压不同,我们需要采用AC耦合,将driver端的输出共模电压去除,然后在靠近receiver端通过分压电阻重新建立满足receiver端的共模电压,如果光模块内部已经建立好了共模电路,则外部就不需要重新搭建电路了。
  • 您好,我们采用的光模块不兼容VML。另外,我们的开发板已经搭建好了,所以更改电路的方案可能不太有操作性。

    而我们采用的能通信成功的DAC线缆是兼容Intel的,通信失败的10G光模块内部使用的是标准码,要是我们使用兼容Intel的码的光模块是否可行?