多种颜色段码数码管显示是如何实现的?不同颜色数码管压降不一样,限流电阻如何确定。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
基本RS触发器的用途之一是作无抖动开关。当开关接通时,由于机械按键开关在扳动的过程中,存在接触抖动,使得输出点电压从+5V直接地跃降到0V的一瞬间(几十毫秒),会发生多次电压抖动,相当产生连续多个脉冲信号。如果利用这种电路产生的信号去驱动数字电路,则可能导致电路发生误动作。这在某些场合是绝对不允许的,为了消除机械开关的抖动,可在开关与输出端点之间接人一个RS触发器,就能使F端产生很清晰的阶跃信号。那么这种带RS触发器的打关通常称为无抖动开关(或称逻辑开关)。而把有抖动的开关称为数据开关。838电子
原理:在按压按键时,由于机械开关的接触抖动,往往在几十毫秒内电压会出现多次抖动,相当于连续出现了几个脉冲信号。显然,用这样的开关产生的信号直接作为电路的驱动信号可能导致电路产生错误动作,这在有些情况下是绝对不允许的。为了消除开关的接触抖动,可在机械开关与被驱动电路间接的接入一个基本RS触发器,如图1所示838电子。S为 =0, R=l,可得出A=l, A=0。当按压按键时,S=l,R=0,可得出 A=0,A=1,改变了输出信号A的状态。若由于机械开关的接触抖动,则R的状态会在0和1之间变化多次,若 R=l,由于A=0,因此G2门仍然是“有低出高”,不会影响输出的状态。同理,当松开按键时, S端出现的接触抖动亦不会影响输出的状态。因此,图1所示的电路,开关每按压一次,A点的输出信号仅发生一次变化
1. 使用限流电阻:V_IO=I*R_limit+V_LED,这种方法的问题是,V_LED跟温度有关,启动瞬间的压降比较高,启动后压降会降下来,所以可能会有色差变化
2. 使用恒流驱动。电流很稳定,但成本高。