应用是这样的:
单片机通过PWM控制led驱动芯片调节占空比,实现电流变化,占空比是0-100。
此LED的工作电压电流是:电流为3A时电压4.5V,电流为2.5A时,电压4V。
外部输入电压为24V,电流足够。
此恒流源驱动工作温度要求:零下40度到125度或者150度。
引脚外置,非QFN等封装,可手动焊接。
要求恒流源芯片为降压型,输出电流最大可以到3A-4A,输出电流可能设计到2.8A或者3A。单路输出即可。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应用是这样的:
单片机通过PWM控制led驱动芯片调节占空比,实现电流变化,占空比是0-100。
此LED的工作电压电流是:电流为3A时电压4.5V,电流为2.5A时,电压4V。
外部输入电压为24V,电流足够。
此恒流源驱动工作温度要求:零下40度到125度或者150度。
引脚外置,非QFN等封装,可手动焊接。
要求恒流源芯片为降压型,输出电流最大可以到3A-4A,输出电流可能设计到2.8A或者3A。单路输出即可。谢谢
你好,
可以参考LM3409,MOS管外置,输入电压范围6V -- 42V,也有高压版本可以支持到75V的输入电压,支持模拟调光/PWM调光。
你好,
建议PWM的电平,与R3上拉电压的电平要匹配,否则上拉电压会通过R3与PWM管脚形成导电通路。
另外,要结合Q3/Q3的VGS导通电平选择合适的上拉/pwm驱动电压。