This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3429 buck-boost,肖特基二极管很烫

Other Parts Discussed in Thread: LM3429

  HI TI enginner

目前我在开发一个货车前大灯的案子

输入18-32V 输出1.3A 26V 

MOS使用30A 100V TO-252封装

肖特基使用 20A 100V TO-277封装

电感使用22uh 饱和电流8A

设定开关频率 700khz

请帮忙分析一下如下问题,谢谢

1. 肖特基很烫,常温下达到了100℃

2. 设定频率为700khz,为何实际测试只有600khz,请帮忙看看如下的波形是否正确。

3. 实际测试效率85%,为何肖特基还是很烫,有没有方法改善。