目前使用TPS53355电源芯片,实际输入电压12V,输出3.3V,电流约15A。通过WEBENCH软件设计原理图,在WEBENCH软件中设置如下,Vin:11V(min)~13V(max),Vout:3.3V,Iout:15A,Ambient Temp:30℃。WEBENCH软件给出的原理设计图中,TPS53355芯片VFB管脚(0.6V)外接电阻38.3k到Vout和10k电阻到GND,算出Vout为2.9V,不是设计想要的3.3V,请问WEBENCH哪里设置错了?哪里还需要设置?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前使用TPS53355电源芯片,实际输入电压12V,输出3.3V,电流约15A。通过WEBENCH软件设计原理图,在WEBENCH软件中设置如下,Vin:11V(min)~13V(max),Vout:3.3V,Iout:15A,Ambient Temp:30℃。WEBENCH软件给出的原理设计图中,TPS53355芯片VFB管脚(0.6V)外接电阻38.3k到Vout和10k电阻到GND,算出Vout为2.9V,不是设计想要的3.3V,请问WEBENCH哪里设置错了?哪里还需要设置?
看了一下datasheet中24/25页,按照公式计算结果,Vfb会比0.6V高一点。WEBENCH给出的高边、低边电阻分别为38.3K、10k,这要选择电阻的话,输出还是不能达到3.3V。