This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LED驱动选型

Other Parts Discussed in Thread: LM3402, LM3429, TPS92691, LM3406, TPS40211, TPS61500, LM3421, TPS54201, TPS54200

12VDC输入,4路LED需要4颗芯片,驱动电压分别为15V 19V 20V 22V,驱动电流都是0.7A,要求能PWM调光。之前用LED6000,发现有很多问题,技术支持也不能解决,然后就用WEBENCH设计:1、TPS92691看了论坛讨论,说有频闪问题,所以PASS;2、LM3429做了热仿真和PWM调光仿真波形稍差,论坛也有反映发热和不适合PWM调光的,但都没有合理解释,所以待定;3、LM3406,这颗是ST的代理推荐我的,而且LM3402口碑不错,但是这颗是BUCK降压,我还要单独为他配个30V的电源,所以待定。以上三颗就是我目前有所了解的,不知道有哪位大神有更合理的方案推荐?拜谢。