This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

日间行车灯型号推荐

Other Parts Discussed in Thread: TPS40211

一.低配版:

  1. 输入电压范围:9V-16V,建议输入电压范围为5V~27V或更大范围。
  2. 工作电压:12V;测试电压:13.5V
  3. 负载:每颗3V 、150mA 白光LED。共30颗。串并联方式不限。
  4. 驱动要求:恒流。
  5. 拓扑原理:建议选用SEPIC 或 BUCK-BOOST。
  6. 其它要求:1.PWM亮度调整。

二、高配版:

30颗LED的点亮方式需为流水点亮,流水方式为1~30依次点亮。对此需要预留逻辑控制功能。

三:元器件要求:

  1. 车规级
  2. 芯片及其它元器件耐温需不小于-40℃~150℃。
  3. 优先选择具有成熟用法的芯片及方案。
  4. EMC兼容性(建议不要选择较高开关频率防止EMC不合格问题)。