This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Many questions for IR-LED driver_1, LP55231

Other Parts Discussed in Thread: LP55231

hi all 

我想請教一下LP55231 硬體的接法(ASEL0,ASEL1,GND)

現在控制9顆IR-LED 1.43V 13.3mA 

希望能有3種操作方法

(1)一顆一顆各別控制,

(2)全亮

(3)做 120HZ 25% duty cycle

請問.

1.現在I2C控制,請問setting 要下那些設定才能enable 55231 ,才能控制D1,~D9?

   可以提供address(64/65) register 給我參考嗎?

2如果要全亮.要下甚麼setting

   可以提供registor給我參考嗎?

3.要做duty cycle? 硬體電路要接 INT pin 還是 TRIG pin?

4.硬體電路上 EN pin 有voltage 的範圍嗎?

   假設EN 接3V3 ,那I2C 的準位就要3V3嗎? 如果EN 接1V8 ,那I2C 的準位就要1V8嗎?

 Thanks

  • Hi

        ASEL0,ASEL1,GND设置I2C地址,见datasheet第18页。

        1. 主要是EN和I2C控制,地址可以看18页。

        2. 寄存器设置,100%调光亮度即可。

        3.通过I2C调光控制。

        4.是得,你看参数表即可,I2C是参考EN电平。不过一般I2C都是3.3V,即便你EN是1.8V,3.3V也应该兼容,因为3.3>0.8*Ven.