Hi TI工程师:
UCC25710的DIM调光信号 以前使用一直是200HZ左右的输入,有个客户,做杜比认证的时候 把这个输入频率调到了将近400HZ;
1:400Hz输入会有问题吗?
2:在规格书上未找到这项说明,帮忙咨询,UCC25710最大输入DIM是多大?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
一般的调光频率都是200Hz,这个芯片datasheet没有说明最高调光频率是多少,但是估计1kHz内应该是没有问题的。
而datasheet 案例的调光频率就是300Hz+/-10Hz,400Hz芯片这边肯定是没有问题。
调光频率还要结合你屏幕的应用,200Hz没有问题,将频率调高,即便异常也不会严重,也就是闪屏之类异常。