HI 你好,
我通过MY DESIGNS防真,用LM5122做了一个12V输入,22V输出的电路,后面接的是TPA3118,60W,
有一个地方令我困惑的是,当TPA3118用1KHZ播放时,功率能达到60W;当TPA3118用100HZ播放时,功率超过来30W时,LM5122就不升压了。
所用硬件都是一样的,但是在低频播放LM5122就工作不正常。以下是原理图和PCB:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI 你好,
我通过MY DESIGNS防真,用LM5122做了一个12V输入,22V输出的电路,后面接的是TPA3118,60W,
有一个地方令我困惑的是,当TPA3118用1KHZ播放时,功率能达到60W;当TPA3118用100HZ播放时,功率超过来30W时,LM5122就不升压了。
所用硬件都是一样的,但是在低频播放LM5122就工作不正常。以下是原理图和PCB:
Hi Johnsin,
找到原因了,是COMP脚的电阻设置不合理,我在MY DESIGN防真出来推荐用的是否12K,会出现以上的状况。
当我把这个电阻换成24K,低频也能加满载了。
规格书上的这一点计算公司说的有点复杂,你能简单点跟我说一下,COMP脚的电阻电容的设计计算吗和如果取值不对,会出现什么状况?