TI 工程师
DRV10983Q1 tune guide
2.2 Motor Resistance
For a wye-connected motor, the motor phase resistance refers to the resistance from the phase output to
the center tap (RPH_CT). This resistance is labeled as RPH_CT in Figure 2.
RY
RY
RY
Rû
Rû
Rû
Center
Tap
Phase U
Phase V Phase W
Phase V Phase W
Phase U
RPH_CT
RPH_CT
RPH_CT
Center
Tap
www.ti.com Acquire Motor Parameter
SLVUAV9 –June 2017 3
Submit Documentation Feedback
Copyright © 2017, Texas Instruments Incorporated
DRV10983-Q1 Tuning Guide
Figure 2. Wye-Connected Motor Resistance
For a delta-connected motor, the motor phase resistance refers to the equivalent phase to center tap in
the wye configuration. In Figure 3, this resistance is calculated as RY × RPH_CT = RY.
For both the delta-connected motor and the wye-connected motor, the easy way to get the equivalent
RPH_CT is to measure the resistance between two phase terminals (RPH_PH) and then divide this value by
two: RPH_CT = ½ RPH_PH.
请问其中delta-connected 的 RY × RPH_CT = RY.这电阻值RY怎么算?用多少来计算,是否有问题?