我想把AWR1443的ADC获取的数据直接进行送到FPGA进行分析,我了解到原始数据可以通过CSI口传输出来,同时,我已经做了一个mipi60pin转FMC的转接板,以使CSI能被FPGA获得。但是我不会配置1443的R4F(MCU)。
1.请问有哪些资料可以参考。
2.另外我注意到mmwave_sdk_02_00_00_04\packages\ti\drivers\test\csi_stream\xwr14xx文件夹下面有一个mss.c的文件,请问这个文件是否可以直接拿来用做MCU上的程序。
3.在用外部FPGA进行数据处理的过程中,这EVM上的R4F(MCU)需要考虑和FPGA有哪些同步吗