中文:
我将iwr1843boot连接到windows上,识别出了两个端口,分别为XDS110 Class Application/ User UART (COM8) 和XDS110 Class Auxiliary Data Port (COM7);当我在ubuntu上编译程序后,将iwr11843boot连接到Ubuntu上,通过lsusb命令查看,却只识别了一个为:Bus 002 Device 006: ID 0451: bef3 Texas Instruments, Inc。然后运行程序,提示如下:
QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
Serial Port Found
Data Port Number is "ttyACM0"
User Port Number is "ttyACM0"
Data port succesfully Open
User port did not Open
请问如何解决这个问题?
English:
When i make iwr1843boot connect to windows, it has two ports,they are XDS110 Class Application/ User UART (COM8) and XDS110 Class Auxiliary Data Port (COM7);When i have builded project and make iwr1843boot connect to Ubuntu, it has one port named by Bus 002 Device 006: ID 0451: bef3 Texas Instruments, Inc with lSUSb command。And when i run my project ,it tell me this message:
QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
Serial Port Found
Data Port Number is "ttyACM0"
User Port Number is "ttyACM0"
Data port succesfully Open
User port did not Open
How to solve this problem please?