你好,我想请问一下
DCA1000将ADC数据存在2GB的缓存中,如果我的帧数太多导致2GB不够,会发生什么情况?
我看到DCA1000中的文档介绍,支持插入一张8GB的SD卡,请问要如何操作?
非常感谢您的解答
你好,我想请问一下
DCA1000将ADC数据存在2GB的缓存中,如果我的帧数太多导致2GB不够,会发生什么情况?
我看到DCA1000中的文档介绍,支持插入一张8GB的SD卡,请问要如何操作?
非常感谢您的解答
ADC数据率小于网口吞吐率,可以实时传输。
默认配置为325Mbps。如需更高,可参考文档以下描述
In default conditions, Ethernet throughput varies up to 325 Mbps speed in a 25-μs Ethernet packet
delay. The user can change the Ethernet packet delay from 5 μs to 500 μs to achieve different
throughputs, as explained in Table 19, to achieve different Ethernet throughputs.
Table 19. Theoretical Throughput
Ethernet Packet Delay Theoretical Throughput (Mbps)
5 μs ~706
10 μs ~545
25 μs ~325
50 μs ~193