TI的技术,你好,现在我正在调试TPS43061升压电路,+24V输入,+48V输出,按照设计输出电流3.125A。但是现在遇到的问题是输出功率最大为30W左右,开关频率770K,外围MOS选用BSC123N08NS3G,输出电感选用IHLP6767GZER3R3M11(3.3uH@27A);我试过带100W负载,输出电压会抬升到63V左右,不清楚为什么,调试期间也烧过1块片子,我想请问一下输出功率上不去,是因为什么原因导致的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI的技术,你好,现在我正在调试TPS43061升压电路,+24V输入,+48V输出,按照设计输出电流3.125A。但是现在遇到的问题是输出功率最大为30W左右,开关频率770K,外围MOS选用BSC123N08NS3G,输出电感选用IHLP6767GZER3R3M11(3.3uH@27A);我试过带100W负载,输出电压会抬升到63V左右,不清楚为什么,调试期间也烧过1块片子,我想请问一下输出功率上不去,是因为什么原因导致的?
你好,你的输出电压调到63V是什么情况,这基本会烧芯片的,SW不能超60v(极限值),谢谢。
你的问题描述的不是很清楚,谢谢。
Hi
可以用这颗芯片,电路可以用TI Webench仿真。
问题可能出在layout上,能否提供输出电压波形? 或者说你得到的63V是稳定电压吗?