用LM5175做一个升降压电路,输入电压20-29.6V 输出电压28V 最大电流为7A。假设输入电压为26V时能够正常稳定输出28V 7A,当调整输入电压变低时,输出电压也会跟着变低。但是如果一开始给个低的电压,则能够稳定输出28V 7A。因为是用电池作为输入,电池的电压会随使用时间降低,附件为原理。麻烦帮忙看下哪里问题!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用LM5175做一个升降压电路,输入电压20-29.6V 输出电压28V 最大电流为7A。假设输入电压为26V时能够正常稳定输出28V 7A,当调整输入电压变低时,输出电压也会跟着变低。但是如果一开始给个低的电压,则能够稳定输出28V 7A。因为是用电池作为输入,电池的电压会随使用时间降低,附件为原理。麻烦帮忙看下哪里问题!!
如果改用外置电源供电,调节输入电压,输出也会有同样的情况出现吗?
在将输入电压降低的实验当中,起始时LM5175是工作在buck-boost模式,到最后是工作在buck模式吗?
你是否方便观察下,当调低输入电压的时候,对应的两个SW节点波形,看看其占空比的改变是否正常
你好,能否观测一下SW1和SW2处的波形,看下LM5175是在什么电压下,从buck-boost模式切换到boost模式的,看下切换前一刻两个SW波形