@TI技术支援团队。在使用LM2519的时候遇到一个问题,25119的耐压是42V,但是我有一款电源的输入电压会到80V, 那么我能不能先25119的供电前做一级42V以内的稳压来解决 ?这样,我仍然能用LM25119来做生产 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
@TI技术支援团队。在使用LM2519的时候遇到一个问题,25119的耐压是42V,但是我有一款电源的输入电压会到80V, 那么我能不能先25119的供电前做一级42V以内的稳压来解决 ?这样,我仍然能用LM25119来做生产 ?
Hi,
您好,你是说LM25119的输入电压可能会达到80V对吗?
首先,这个芯片推荐工作电压是40V,42V是极限值,建议将输入电压限制在40V以内。
其次,我认为只要您能保证LM25119 VIN引脚上的电压不超过40V就是可以的。不知您指的80V是不是电压尖峰,可以选择用TVS来抑制这个电压尖峰,但是TVS是将尖峰的能量转化成热释放掉,所以会影响整个系统的效率。选用TVS时还要注意TVS的功率限制能否达到要求。
谢谢!
我是用LM25119做了一款35V转12V 40A的电源,LM25119的VCC是直接经过一个10R的电阻接到35V供电输入端。目前的问题是客户使用环境改变了,输入电压从原来35V要改为80V峰值。我的意思是能不能把LM25119的VCC这里先从80V降压到40V内,这样我就可以继续使用同一个芯片LM25119 ?
Hi,
您指的是VIN还是VCC?原先的设计应该是VIN接到40V吧?VCC是内部regulator的输出,标称电压7.6V,是承受不了40V的。可以看手册上的Block Diagram,VIN经过一个LDO降压成7.6V供给VCC,VCC再去作为驱动器的电源,并且为逻辑部分供电。
另外我猜测您是不是说,因为这是个控制器,所以把80V Vin降压成40V给到芯片上是不是可以工作? 这个是不行的,因为手册上有写SW只能承受45V极限值,就算降到40V,如果用80V作Power VIN的话,SW仍然要承受80V的电压。
如果是瞬时80V尖峰可以考虑用TVS,如果是稳定80V,建议您另选一款别的芯片。
哦,明白了,只把vin稳压成40V内还是不行的,SW仍然有80V。
谢谢了!