This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54821短路的问题。

Other Parts Discussed in Thread: TPS54821

最近用TPS54821 搭了一个电路,输入14V,需求输出5~12V可调,100mV/step,电路设计出来了,调试功能也正确,但是在使用过程中从5V调压到9V或者调压到12V的时候,经常会听到啪声,而且第一次上电的时候经常会出现烧片的问题,烧片后,输入和输出都对地短路了。求TI的大神能够给一些指导意见,急急急!!

  • Hi

           建议首先将电感饱和电流选择大一些,啪声是电感发出来的。

           建议你在DAC输出增加一个二极管,防止在启动时,如果DAC输出是0V,  影响到电源输出。加二极管后,电源按照其反馈电阻输出,DAC输出大于二极管压降加上Vsen电压才能调节输出,这样也是单向调节。

  • 你ADC输出端先加一个RC低通滤波(100p,1K),然后在串一个10K左右的电阻,不要用0欧姆直接串联,这样很容易损坏芯片,因为FB很敏感,一旦电流过大,很容易就坏片