我用TPS43060搭建12V升24V 20A输出,但是现在输出自能够到2A,输出3A电压就会掉,原理图和PCB在附件里面,用的电感是33UH 100A的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用TPS43060搭建12V升24V 20A输出,但是现在输出自能够到2A,输出3A电压就会掉,原理图和PCB在附件里面,用的电感是33UH 100A的
HI
如果确认电感饱和电流100A,你还需要确认如下:
1. layout上功率回路尽量小,以及避免sense电阻noise.
2 .MOS选择Qg尽量小,从PWM确认芯片驱动能力是否足够。
C9取太大了,一般都是pF级别的,建议你按照手册上公式重新计算优化一下
或者直接用WEBENCH软件优化https://webench.ti.com