This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lp5912-1.2V功耗

Other Parts Discussed in Thread: LP5912, TMS320F28377S

使用LP5912进行3.3V转1.2V稳压,给TMS320F28377SZWT内核供电。

3.3V是由5V通过TPS73733稳压过来的。

现在的问题是在TMS320F28377S是空片的情况下,上电都有0.2A的电流,1W的功耗。

我的电路外设目前只有两个MAX3490。我把LP2912去掉,上电电流只有0.03A。

这么算的话有约0.17A在3.3V转1.2V的时候消耗掉了,LP5912消耗掉的功率就有约0.17X(3.3-1.2)=0.357W。

这样正常吗?怎么降低呢?