Hi :
调试过程存在如下问题,根据提供的参数计算不可用,可否协助计算下变压器和OVP和Rcs等外围器件参数?
1 输入18-36V DC
2 输出8.2VDC 30W
3.变压器TR参数
磁芯:PQ2016
匝比:Pri : Bis : Sec=12:12:7
感量:65uH
可否提供下变压器及其他外围器件参数,目前根据官网提供资料计算不正常;
1.调试过程中,加载0.1A,驱动波形和CS波形如下:
2.OVP上下段电阻和Rcs、Rpl的参数如何计算,可否提供下?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.