This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331不同负载纹波情况

Other Parts Discussed in Thread: TPS54331, TPS562209

感谢TI和MPS提供可靠的电源芯片。

在项目中大量使用性价格高的DCDC芯片-TI的TPS54331和MPS的MP1470。

之前产品对 高度没有限制所以使用的输入输出电容皆为点解电容,后来由于结构限制输入输出电容更换为MLCC电容,负载是数码管驱动芯片,驱动2-8位数码管。

板子是先通过TPS54331把24V转为12V,然后通过MP1470将12V转为5V,数码管驱动芯片是5V,全部点亮数码管电流大约在300mA.

当我点亮数码管后,PCBA上发出滋滋的啸叫声。我把数码管驱动芯片吹掉,在5V上接入水泥电阻,接近满量程纹波也在接受范围内,没有啸叫;我把MP1470吹掉,在12V接入水泥电阻,也是正常。但是即使只点亮一个数码管也会有啸叫,并且纹波急剧变大,大约800mV+,频率1khz左右。

这种情况实际上负载很小,但是水泥电阻的情况和数码管驱动芯片的情况完全不同。

我通过把12V和5V上的MLCC电容换成点解电容会缓解。

如果还是要用MLCC电容该怎么改进。