This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LM5575外围电路器件选型的若干疑问

Other Parts Discussed in Thread: LM5575

你好,目前选用贵司的LM55751.5A版本)做为板子的主电源芯片。我的输入电压范围是从8 VDC~70 VDC,输出电压是5.3 VDC,输出电流范围是20mA~150mA,由于走量的原因,只能选择1.5A版本的LM5575,目前有几点疑问如下:

1、通过输出电压知道了反馈电阻的阻值比,但是反馈电阻的具体值该如何选择。Datasheet中这样描述“对于5V输出,电阻应该从标准阻值中选择,最好先从1.0 kΩ - 10 kΩ之间开始选择。”,在AN-1571 Quick Start Guide中这样描述“Set Rfb2 to 5kOhms if Vout[1] is less than or equal to 5 Volts. If Vout[1] is greater than 5V setRfb2 to 10K Ohms.”不过在webench中通过仿真它建议两个电阻阻值是30.9K10.2K

2RAMP的电容该如何选择,datasheet中说通过输出电感选择Cramp,目前输出电感是470μH,那么Cramp应选择4.7nF。然而datasheet中又说推荐的电容范围是50Pf~2000pF。是不是两者相互矛盾了。

3、补偿网络的RcompCcomp的理论值该如何计算,AN-1571 Quick Start Guide中给出了Rcomp的计算公式,总之是由反馈电阻,输出电容,输出电压决定的,真是如此吗?这也是我一直纠结反馈电阻取值的原因。

4、在该论坛提问问题,是不是不能上传图片?

谢谢。