由于PCB板上需要不同电压供电,我需要得到正负15V得电压(给运放供电),正负5V(给74HCT4053多路复用器供电),正3.3V(给DA芯片供电),正2.5V给(AD芯片供电),可以给我介绍相应的芯片吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
非常感谢你的回复
输入电压+24V,正负15V电压最大负载电流300mA,正负5V负载电流100mA,3.3V负载电流50mA,可以给我推荐合适的芯片吗
Hi
非常感谢你的答复,
上述设计+/15V的输出电流有点小,有没有输出电流更大的设计
是和这个文档http://www.ti.com.cn/cn/lit/an/slva369a/slva369a.pdf上的所给的电路结构相同,我只需要改一下芯片,重新计算一下参数,然后就可以应用了吗?