This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR16030

Other Parts Discussed in Thread: LMR16030

你好,

我使用LMR16030设计了一个60V转5V的电路如下,根据公式算出最后输出应该是4.9V左右,但是设计测量输出有5.2V,请问该电路是否存在问题,谢谢。

  • Hi
    首先用示波器测试确认,测试的5.2V是否是稳定的,如果是不稳定的。请问你的输出电容用的是点解电容吗? 建议用低ESR陶瓷电容,如2个47uF的陶瓷电容。
    如果是稳定的,确认反馈电阻的精度。
  • 你好,

    你电路的工作频率接近2MHz,手册上标注的可控最小导通时间是90ns,所以有可能是你的电路降压比太高,可以通过将输入电压调低观察输出是否正常来验证一下。如果是这个原因,可以通过降低工作频率实现更高的降压比。