This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS61021A的应用问题

Other Parts Discussed in Thread: TPS61021A, LM5150-Q1

目前有个项目,设计要求如下:

输入电压:1-3V

输出电压:3.8V

输出峰值电流:2.3A(峰值电流表现为脉冲形式,持续时间约500us,12%左右的占空比)

输出平均电流:200mA

我在TI网站上找了一圈,发现也就TPS61021A这个芯片比较接近了,现在的问题有两个:

1.规格书上说TPS61021输出3.3V时电流为1.5A,我不清楚是否能够承载2.3A的的峰值电流?

2.规格书上建议输出电容最大为200UF,我如果将电容加大到500UF左右,是否会有问题?

谢谢。