This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210测试结果与设计不符

Other Parts Discussed in Thread: CSD18543Q3A, TPS40210

    最近需要做一个12V转48V的电源模块,使用webench设计结果如下图所示

实际设计原理图如下图所示

在实际调试过程中发现几个问题:

1.输出电压不是48V,而是28-30V左右。

2.测量VFB电压为0.45V左右,并不是手册中说的0.7V

3.设计中的CSD18543Q3A测试过程中莫名其妙坏了2只。

实际测试供电12V,无负载,12V电流足够。

实际参数C5为2.2uF,R5为9.1R,R4,R7未焊接,其他与设计原理图一样。