This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5050冗余设计出现疑似倒灌

Other Parts Discussed in Thread: LM5050-1, TPS2660

大家好,我在使用LM5050做电源冗余设计的时候,遇到一个问题如下:

右边输入为一个高压DC-DC隔离模块,同样输出50V。主要想实现的功能为,当高压DC-DC模块出现故障时,切断输出,使用另外的一路50V输入作为输出。在目前的测试过程中遇到一个问题,当我使用一台800V的高压稳压源为DC-DC隔离模块供电,50V的低压稳压源做in_50,那么在同时启动两个稳压源的情况下,50V的低压稳压源输入会使DC-DC模块保护,此时DC-DC模块无输出。当关闭50V的低压稳压源后,DC-DC模块正常输出50V。此处怀疑,是否上述LM5050冗余电路存在倒灌的可能,致使DC-DC模块故障保护?

注:此电路使参考论坛中部分坛友测试说明,在VS接输出端无法正常进行冗余工作后将VS接输入端使用!

  • 请提供相关的电压与电流波形。

    If the MOSFET current reverses, possibly due to failure of the input supply, such that the voltage across the LM5050-1 IN and OUT pins is more negative than the VSD(REV) voltage of -28 mV (typical), the LM5050-1 will quickly discharge the MOSFET gate through a strong GATE to IN pin discharge transistor.

  • 理论上不会吧,否则就失去了这个IC的意义,你可以这样测试下:
    1、只接左边电源,右边的DC-DC不启动,启动左边电源后,看右边电源输出端电压多少?
    2、将右边DC-DC去掉,换成一个大阻值电阻,启动左边电源后,看左边电源输出多少。
    3、如果时第一步能测到电压,第二步测不到电压,那么可能时MOS管体导致,在你目前电路右边DC-DC输出加一个死负载再试试。
  • Hi
    你的意思是低压源的50V会导致高压源的50V电源电路关机吗? 即便前者先启动MOS的二极管应该会使其隔离开,相当于高压部分空载启动。 建议你从波形上看。
  • 你好,按照你的建议我做了几个测试,详情请见附件!相当于LM5050并没有将回路彻底关断,因为还有体二极管的存在。那么我现在有一个问题就是,LM5050是否可以设计双N-MOSFET背靠背防倒灌电路呢?如下:

  • 同样麻烦您看下,有关LM5050的应用,是否可以进行双N-MOSFET背靠背防倒灌设计呢?谢谢!
  • 首先这不是倒灌,这是正常现象。LM5050是ORING线路,其主要目的就是做一个理想的二极管作用,即需要MOS管体二极管导通时,芯片控制驱动将MOS管完全导通来降低功耗。
  • 谢谢您关注这个问题!
    我做的这两个实验只是证明了不能彻底关断回路。因为之前测试损坏了一个高压DC-DC模块,价格比较昂贵,故这次使用电池做替代,之前的测试也是使用电池的情况下,电路工作正常。出现问题的只是高压DC-DC模块双电源切换时会出现这个问题。
    那么就像我在上面说的,是否可以用双N-MOSFET组成防倒灌电路呢?我刚刚搭了一个简易的电路,测试在LM5050的OFF端+5V高电平的时候,GATE引脚电平与输入电压基本相同,但是回路还是没有关闭,这点想不通!
  • LM5050不支持背靠背MOS的方案。如果电流不大,可以看一下TPS2660。
  • 非常感谢您的建议。但是我这边需求回路电流>100A,所以必须使用外置MOS,只能找找能驱动背靠背MOS方案的IC了!