This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175欠压锁定,Vcc电压处于3.3V,输出电压为几百mV?

Other Parts Discussed in Thread: LM5175

Hi,Ti专家以及各位大牛:

        在调试LM5175出现如下现象,望大牛给些指导,我们电路设计思路:输入电压为12V,通过DAC、运放以及外围电路构成电压反馈回路,实现输出电压连续可调,可调范围3V~50V。在调试过程中发现,通过控制DAC输出使LM5175输出3V至10V电压,均正常,Vcc为7.4V左右,FB引脚电压在0.8V左右,当控制使其输出15V电压时,FB引脚电压为0.67V,Vcc电压也不正常,返回去又控制DAC使其输出3V电压,实测为2.5V左右;重新上电配置,测得LM5175输出均为几百mV,Vcc电压稳定在3.3V,查看手册,此时应该处于欠压锁定状态,望大牛指导,这种现象该怎么解决?附件为原理图。