This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求推荐 15V OR 24V输入,+12V( 1.5A) and +5V (2A)输出,纹波小点的

Other Parts Discussed in Thread: TPS54386, TPS54202H, LMR23630, TPS54202, LM5160, LM5160-Q1

您好!

      15V OR 24V输入,+12V( 1.5A) and  +5V (2A)输出,纹波小点的,请问有哪些性价比比较高的?谢谢!