This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于UCC28780使用的疑问

Other Parts Discussed in Thread: UCC28780

TI的工程师:

您好!

目前想用UCC28780作为PWM管理芯片做一款45W的TYPE_C接口 PD快充。输入电压范围:85-265V AC,输出电压/电流:5V/3A、9V/3A、12V/3A、15V/3A,

20V/2.25A。最小开关频率频率应该在5V/3A下确定还是20V/2.25A确定?

另外数据手册中频率的计算公式中(公式29),为什么除了有四分之一的谐振周期还有Im从负到零的时间,谐振周期中就是让电流从负变成零了吗?

假设最小频率为200K,使用公式23计算出来励磁电感LM,再代入到公式29中,计算出来的频率远小于200K。

可否帮忙解答一下这几个疑问?