This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA282應用諮詢

Other Parts Discussed in Thread: INA282

HI,

有個INA282的應用問題想請教:

补充下客户运用场景:当电流从左向右时,要输出一个高电平(大于1V);当电流为0V和为从右向左时,要输出一个0V电压或者是小于0.5V的电压;用来解决PMOS管的电流反灌的

1,采样电阻两端的差分电压值范围是多少?

2,GAIN增益值是拿来做什么的?

3,采样电流与输出电压的计算公式是怎样的?

4,如果接成单向电流从左向右的接法后,在实际使用时出现电流从右向左的状态时,输出电压是什么状态,如果检测电流为0的时候状态又会是什么样?

以上問題,想諮詢下

謝謝

  • Hi
    建议将问题放到“放大器”对应论坛讨论,这里主要是针对电源芯片。
  • 1、采样电阻两端的差分电压=负载电流*采样电阻值
    2、INA282是一个固定增益(50倍)的运放,增益就是运放的放大倍数。
    3、采样电流*采样电阻*50=输出电压(INA282的输出电压)
    4、这个取决于参考电压的设定(REF1和REF2),参考电压口接地,输出电压只能检测正向电流,参考电压不为零,输出电压可以体现双向电流的流向。比如REF1接地,REF2接5V,实际内部运放的参考电压为2.5V,则,输出电压>2.5V,说明电流方向为从左到右;输出电压<2.5V,说明电流方向从右到左。输出电压为2.5V,代表检测的电流为零。
    我的解释你还满意吗?