This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62163 EN端电压异常问题

Other Parts Discussed in Thread: TPS62163

电路图如上所示,C点处,即EN端的电压出现了一个无法理解的值。

首先,整个系统输入输出都是正常的,输入12V,输出5V。A点B点分别为控制EN端的两个输出。

实际测得A点、B点电压为3.3V,

但C点电压为3.5V。。。

两个2极管也正常(在TPS62163非通电,A,B与C呈现正向导通,并有0.01V左右的压降。

不知道C点为何在TPS62163工作的情况下电压会高于A,B两点。