客户设计的规格为输入是9~36V,输出是12V, 10A; 目前客户在调试过程中遇到的问题是,输出电流为6A, 12~22V输入都是正常的。 当输入为23V以上时,输出变成13V了,PGOOD不输出。当调回22V时,输出为12V,其他什么的都正常了。下图为客户原理图。客户想了解是什么原因造成这个问题,该如何解决。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
客户设计的规格为输入是9~36V,输出是12V, 10A; 目前客户在调试过程中遇到的问题是,输出电流为6A, 12~22V输入都是正常的。 当输入为23V以上时,输出变成13V了,PGOOD不输出。当调回22V时,输出为12V,其他什么的都正常了。下图为客户原理图。客户想了解是什么原因造成这个问题,该如何解决。谢谢!
Hi
处在降压模式下,输入电压越高,电感的峰值电流越大,layout不好寄生参数造成的干扰也越大。
建议你确认一下反馈的GND以及layout.(GND选择模拟GND)
目前我们发现FB的管脚的电压不能锁定,当电压输入为24V时,FB的电压为0.865V,输出变成了13V,PGOOD无输出;当输入为19V时,FB的电压为0.8V,输出就是12V;请问这个现象能确定就是LAYOUT的问题吗?