This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176 23V以上 输入时 输出电压升高,PGOOD无输出的问题

客户设计的规格为输入是9~36V,输出是12V,  10A;  目前客户在调试过程中遇到的问题是,输出电流为6A, 12~22V输入都是正常的。 当输入为23V以上时,输出变成13V了,PGOOD不输出。当调回22V时,输出为12V,其他什么的都正常了。下图为客户原理图。客户想了解是什么原因造成这个问题,该如何解决。谢谢!