This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65150 无输出

按照参考电路设计,需求:VS=12V  VGH=20V VGL=-10V  输入:5V   电路如下:其中330nf均换为470nf 

问题描述:轻载情况下,输入正常5v   SW (pin 5 6 )输出在极短时间内大致为13V左右的不规律波形(用两块板子试验 ,瞬间电压相同,频率从60k-240k不等),之后为持续的5V 电平  5v稳压源显示上电瞬间为24mA左右电流

已进行操作为:将R78 79 73 74 取下,只留FB一个馈点;将R81 R80 取下,GD悬空;确定所用电容满足电压条件。