This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256301反复自启

Other Parts Discussed in Thread: UCC28180, UCC256301, TL431

UCC256301搭配PFC:UCC28180,上电经常不正常,后来改了环路上供给光耦的电流,空载电压为45V,稍微带100mA电流就没有输出,改了一下TL431的反馈RC数值后,启动又不正常了,感觉像是反复自动,是什么原因呢?波形如附件,CH1是低管驱动脚,CH2是软起动脚,CH3是FB脚。

  • Hi

        首先PFC是否正常输出?

        如果是UCC256301输出不正常,也就是完全带不动负载,是吗?  确认一下变压器和保护电路?

  • 软起动重复启动,如果没有保护起作用,那就是布局不合理,IC收到了干扰造成IC自身不停的启动。
  • PFC工作正常,UCC256301工作不正常,输出跳变,也带不起载。变压器参数如:励磁电感270uH,谐振电感57uH,谐振电容47nF。感觉在启动的过程中都不怎么对劲,请见附件下管驱动波形及VCR脚的波形。

  • 跟DEMO的区别就是把IC的小信号地和功率管的大电流地分开到电解电容汇合,然后就是因为结构不一样,管子的放置不同,不对请指出,谢谢!。