This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118 buck-boost电路 带负载能力差 的问题?

Other Parts Discussed in Thread: LM5118

如下图,为 使用TI WEBENCH生成的 buck-boost电路,主控IC为LM5118。
参数如下


输入电压范围:DC22.0V-DC45V ;
输出电压:DC24.0V ;
输出持续最大电流:2.0A 。

调试时,测试数据如下:

1.无负载时
输入电压:DC19.60V ;
输出电压:DC24.12V ;

2.带49.33Ω负载时

输入电压:DC19.61V ;
输出电压:DC15.62V。

总结:
无负载时,输出电压正常(DC24.12V);
带49.33Ω负载时,输出电压 为:DC15.62V 。

请问:
负载并不大,为什么 输出电压 不对 ?

非常感谢!