This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61088无法关断

Other Parts Discussed in Thread: TPS61088

使用了官网上的软件建议,设计了一个锂电池升压到12V,提供2A的电流,试图通过一个触摸开关控制芯片的EN脚来关闭电源,但是发现无法关断,输出仍然有3.4V(此时锂电池3.8V),这个3.4V有非常大的带载能力,我用夹子夹住输出电容C16,可以将焊锡融化。

为了排除是控制电平问题,测量电压是非常接近于0V的,索性又对EN脚去掉电阻直接连接到GND,但是仍然有输出;本方案电源输出主要用于无电供电装置,怀疑无线供电有辐射作用,去掉线圈发现还是仍然没有起到作用,对此很疑惑,请教是还有什么原因存在?

   下图中没有体现出热焊盘连接,实际PCB是有设计连接,参考官方layout建议设计。

  • Hi

        升价芯片从输入,到电感,到肖特基,到输出会形成通路,即便芯片不启动,这个通路也不会关闭,所以TPS61088输出会有电压,并且电压值为Vin-Vf(肖特基压降,忽略电压DCR产生的压降)

        为了解决这个问题,很多芯片将肖特基改为背靠背肖特基,这个可以在芯片不启动时关闭输出,但TPS61088不是这样的设计。

        所有你可以增加关断控制电路,或者选择一款靠背肖特基的升压芯片。

  • 嗯嗯,我分析了IC的内部原理框图,也是猜测同样的原因导致,感谢。
  • Hi,

    可以参考芯片datasheet的第9页,芯片内部结构框图。可以看到输入源经过电感之后会经过内部的NMOS(注意其方向)的体二极管,最终会看到Vout上也有VIN减去这个二极管的压降。

    有效的方法是换一个内部是背靠背结构的boost芯片,或者是在VIN端加入一个E-fuse,如TPS2594X等,可以有效阻断该通路。