我想要设计一款负压源:输出-30V~-75V之间,输出范围更大更好。最大输出电流1A左右就行,输入电压范围没有要求,固定一个输入电压就行。要求输出电压可以外部控制,在-60~-75之间可以连续调节,外部控制最好是数字控制,而不是依靠改变取样电阻的方式改变输出电压。输出纹波理论上可以达到100mV一下。用LM5164能不能实现??如果不能,请推荐几个可用芯片。MAX1847可以直接输出负压,但是我不清楚是否可以外部数字控制改变输出电压?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.