This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3402输出电压及输出电流计算的问题

Other Parts Discussed in Thread: LM3402

图1  测试电路图

根据论坛里朋友的指点,我分别测量了CS端 、SW端 、 VIN端 、A点(即 L2 与C42接点)的信号,下图2为CS端与SW端示波器测量图 , 下图3为SW端与A点信号图

图2  LM3402芯片CS点(红)与SW(黄)信号波形

图3    SW点(黄) 与 A点(电感后级)信号图

之后我又测量了VIN(+12V)端 ,12V电压稳定。

我有以下疑问:

1、在DIN始终拉高的情况下 ,SW的频率(1MHz,Ton = 710ns , Toff = 290ns)是由什么决定的?

2、根据手册描述CS端应该始终是200mV ,但是根据图2所示波形(红线)却不是稳定电压,这是为什么 ?

3、根据Iled的计算公式,IF = RSNS*0.20V + ((VIN - VOUT)/ 2L)* (tON) - (VOUT x tD)/L  ,计算得 Iled = 212mA , 但是实际测得电流仅为30mA ,不知道问题出在哪里?!!

  请提供一下帮助!谢谢!